Ir para o conteúdo principal

Network Connections - Base de Conhecimento / Products / HiMobile - Belden Support Center

Network Connections

As of HiMobile version 2.0 next to devices also network connections and their properties are available.

HiMobile Home Screen


Click on Network to browse the project tree.

Project / Folders


Select a project and subfolder to display the device/connections list.



The connections can be found below the device list.
Select one to display the connection properties.


There are two screens. Wipe left/right to change between them.