Ir para o conteúdo principal

I do not receive SMS from OWL. Why? - Base de Conhecimento / Products / OWL - Belden Support Center

I do not receive SMS from OWL. Why?

There might be several reasons:
  1. Phone number of "SMS Service Center" is not entered. In web IF use menu "Administration - Set SMS Service Center"
    Please note that the SMS Service Center at release 1.0.0 is not displayed in the web IF.
    You can check the entered number using SSH with command
    sudo gsmat "AT+CSCA?"
    valid for OWL-3G and OWL-LTE
  2. Wrong phone number. Please enter the number without dashes or slash.
  3. Not enough credit on prepaid card
  4. Not enough transmit power