Ir para o conteúdo principal

How can I use HiMobile to access Industrial HiVision outside of my local Wifi network, e.g. on remote sites? - Base de Conhecimento / Products / HiMobile - Belden Support Center

How can I use HiMobile to access Industrial HiVision outside of my local Wifi network, e.g. on remote sites?

The full feature set of HiMobile is only available, if the device running HiMobile can access the Industrial HiVision webserver. If you are on a remote site with only cellular connection (or other Wifi granting internet access) available, you can still access your Industrial HiVision webserver using a VPN connection. If your VPN grants you access to the machine running the Industrial HiVision services as the local Wifi used for setup does, you can establish a VPN connection with your cell phone, then start the HiMobile app and connect to the server.

Please note: HiMobile needs some bandwith to work smoothly, it can lead to issues if the cellular connection is not fast enough.