Ir para o conteúdo principal

HiMobile Device-, Port- and Connection signaling - Base de Conhecimento / Products / HiMobile - Belden Support Center

HiMobile Device-, Port- and Connection signaling

This lesson describes the signaling feature of HiMobile 3.0

Device Signaling

Device signaling requires HiOS 04.0.00, ClassicSwitch 09.0.01, HiSecOS 03.0.00 or later versions.

In the network overview, tap on the device you want to signal
In the device overview, scroll down to the property „Signaling“ and tap the light bulb
The device will signal like with HiDiscvory for a few seconds

Port Signaling

Port signaling requires HiOS 06.0.01 or higher

In the network overview, tap on the device with the port you want to signal
In the device view, swipe to the left to see the port overview
In the all port overview, tap on the port you want to signal
In the port overview, scroll down to the property „Signaling“ and tap the light bulb

The port will signal for a few seconds

Connection Signaling

Connection signaling requires HiOS 06.0.01 or higher

In the network overview, tap on the connection you want to signal
In the connection overview, scroll down to the property „Signaling“ and tap the light bulb

The two end ports of the connection will signal for a few seconds