Overslaan naar hoofdinhoud

Industrial HiVision 08.1.02 was released - Nieuws / Software Products - Belden Support Center

sep 1 2020

Industrial HiVision 08.1.02 was released

Lijst van auteurs

Security Vulnerability Corrected in version 08.1.02

                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                       

VulnerabilityDescription
Java CVE-2020-2754Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE (component: Scripting). Supported versions                 that are affected are Java SE: 8u241, 11.0.6 and 14; Java SE Embedded: 8u241. Difficult to exploit vulnerability allows                 unauthenticated attacker with network access via multiple protocols to compromise Java SE, Java SE Embedded. Successful                 attacks of this vulnerability can result in unauthorized ability to cause a partial denial of service (partial DOS) of                 Java SE, Java SE Embedded. Note: Applies to client and server deployment of Java. This vulnerability can be exploited                 through sandboxed Java Web Start applications and sandboxed Java applets. It can also be exploited by supplying data to                 APIs in the specified Component without using sandboxed Java Web Start applications or sandboxed Java applets, such as                 through a web service.
Java CVE-2020-2755Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE (component: Scripting). Supported versions                 that are affected are Java SE: 8u241, 11.0.6 and 14; Java SE Embedded: 8u241. Difficult to exploit vulnerability allows                 unauthenticated attacker with network access via multiple protocols to compromise Java SE, Java SE Embedded. Successful                 attacks of this vulnerability can result in unauthorized ability to cause a partial denial of service (partial DOS) of                 Java SE, Java SE Embedded. Note: Applies to client and server deployment of Java. This vulnerability can be exploited                 through sandboxed Java Web Start applications and sandboxed Java applets. It can also be exploited by supplying data to                 APIs in the specified Component without using sandboxed Java Web Start applications or sandboxed Java applets, such as                 through a web service.
Java CVE-2020-2756Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE (component: Serialization). Supported versions                 that are affected are Java SE: 7u251, 8u241, 11.0.6 and 14; Java SE Embedded: 8u241. Difficult to exploit vulnerability                 allows unauthenticated attacker with network access via multiple protocols to compromise Java SE, Java SE Embedded. Successful                 attacks of this vulnerability can result in unauthorized ability to cause a partial denial of service (partial DOS) of Java SE,                 Java SE Embedded. Note: Applies to client and server deployment of Java. This vulnerability can be exploited through sandboxed                 Java Web Start applications and sandboxed Java applets. It can also be exploited by supplying data to APIs in the specified                 Component without using sandboxed Java Web Start applications or sandboxed Java applets, such as through a web service.
Java CVE-2020-2757Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE (component: Serialization). Supported versions                 that are affected are Java SE: 7u251, 8u241, 11.0.6 and 14; Java SE Embedded: 8u241. Difficult to exploit vulnerability                 allows unauthenticated attacker with network access via multiple protocols to compromise Java SE, Java SE Embedded. Successful                 attacks of this vulnerability can result in unauthorized ability to cause a partial denial of service (partial DOS) of Java SE,                 Java SE Embedded. Note: Applies to client and server deployment of Java. This vulnerability can be exploited through sandboxed                 Java Web Start applications and sandboxed Java applets. It can also be exploited by supplying data to APIs in the specified                 Component without using sandboxed Java Web Start applications or sandboxed Java applets, such as through a web service.
Java CVE-2020-2773Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE (component: Security). Supported versions that                 are affected are Java SE: 7u251, 8u241, 11.0.6 and 14; Java SE Embedded: 8u241. Difficult to exploit vulnerability allows                 unauthenticated attacker with network access via multiple protocols to compromise Java SE, Java SE Embedded. Successful                 attacks of this vulnerability can result in unauthorized ability to cause a partial denial of service (partial DOS) of                 Java SE, Java SE Embedded. Note: Applies to client and server deployment of Java. This vulnerability can be exploited                 through sandboxed Java Web Start applications and sandboxed Java applets. It can also be exploited by supplying data to                 APIs in the specified Component without using sandboxed Java Web Start applications or sandboxed Java applets, such as                 through a web service.
Java CVE-2020-2781Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE (component: JSSE). Supported versions                 that are affected are Java SE: 7u251, 8u241, 11.0.6 and 14; Java SE Embedded: 8u241. Easily exploitable vulnerability                 allows unauthenticated attacker with network access via HTTPS to compromise Java SE, Java SE Embedded. Successful                 attacks of this vulnerability can result in unauthorized ability to cause a partial denial of service (partial DOS)                 of Java SE, Java SE Embedded. Note: Applies to client and server deployment of Java. This vulnerability can be exploited                 through sandboxed Java Web Start applications and sandboxed Java applets. It can also be exploited by supplying data to                 APIs in the specified Component without using sandboxed Java Web Start applications or sandboxed Java applets, such as                 through a web service.
Java CVE-2020-2800Vulnerability in the Java SE,  Java SE Embedded product of Oracle Java SE (component: Lightweight HTTP Server). Supported                 versions that are affected are Java SE: 7u251, 8u241, 11.0.6 and 14; Java SE Embedded: 8u241. Difficult to exploit vulnerability                 allows unauthenticated attacker with network access via multiple protocols to compromise Java SE, Java SE Embedded. Successful                 attacks of this vulnerability can result in unauthorized update, insert or delete access to some of Java SE, Java SE Embedded                 accessible data as well as unauthorized read access to a subset of Java SE, Java SE Embedded accessible data. Note: This                 vulnerability can only be exploited by supplying data to APIs in the specified Component without using Untrusted Java Web Start                 applications or Untrusted Java applets, such as through a web service.
Java CVE-2020-2830Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE (component: Concurrency). Supported versions                 that are affected are Java SE: 7u251, 8u241, 11.0.6 and 14; Java SE Embedded: 8u241. Easily exploitable vulnerability                 allows unauthenticated attacker with network access via multiple protocols to compromise Java SE, Java SE Embedded.                 Successful attacks of this vulnerability can result in unauthorized ability to cause a partial denial of service (partial DOS)                 of Java SE, Java SE Embedded. Note: Applies to client and server deployment of Java. This vulnerability can be exploited                 through sandboxed Java Web Start applications and sandboxed Java applets. It can also be exploited by supplying data to APIs                 in the specified Component without using sandboxed Java Web Start applications or sandboxed Java applets, such as through a web service.
Java CVE-2020-14556Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE (component: Libraries). Supported versions                 that are affected are Java SE: 8u251, 11.0.7 and 14.0.1; Java SE Embedded: 8u251. Difficult to exploit vulnerability                 allows unauthenticated attacker with network access via multiple protocols to compromise Java SE, Java SE Embedded.                 Successful attacks of this vulnerability can result in unauthorized update, insert or delete access to some of Java SE,                 Java SE Embedded accessible data as well as unauthorized read access to a subset of Java SE, Java SE Embedded accessible                 data. Note: Applies to client and server deployment of Java. This vulnerability can be exploited through sandboxed Java                 Web Start applications and sandboxed Java applets. It can also be exploited by supplying data to APIs in the specified                 Component without using sandboxed Java Web Start applications or sandboxed Java applets, such as through a web service.
Java CVE-2020-14577Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE (component: JSSE). Supported versions that                 are affected are Java SE: 7u261, 8u251, 11.0.7 and 14.0.1; Java SE Embedded: 8u251. Difficult to exploit vulnerability                 allows unauthenticated attacker with network access via TLS to compromise Java SE, Java SE Embedded. Successful attacks                 of this vulnerability can result in unauthorized read access to a subset of Java SE, Java SE Embedded accessible data.                 Note: Applies to client and server deployment of Java. This vulnerability can be exploited through sandboxed Java Web                 Start applications and sandboxed Java applets. It can also be exploited by supplying data to APIs in the specified                 Component without using sandboxed Java Web Start applications or sandboxed Java applets, such as through a web service.
Java CVE-2020-14578Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE (component: Libraries). Supported versions                 that are affected are Java SE: 7u261 and 8u251; Java SE Embedded: 8u251. Difficult to exploit vulnerability allows                 unauthenticated attacker with network access via multiple protocols to compromise Java SE, Java SE Embedded. Successful                 attacks of this vulnerability can result in unauthorized ability to cause a partial denial of service (partial DOS) of                 Java SE, Java SE Embedded. Note: Applies to client and server deployment of Java. This vulnerability can be exploited                 through sandboxed Java Web Start applications and sandboxed Java applets. It can also be exploited by supplying data to                 APIs in the specified Component without using sandboxed Java Web Start applications or sandboxed Java applets, such as                 through a web service.
Java CVE-2020-14579Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE (component: Libraries). Supported versions                 that are affected are Java SE: 7u261 and 8u251; Java SE Embedded: 8u251. Difficult to exploit vulnerability allows                 unauthenticated attacker with network access via multiple protocols to compromise Java SE, Java SE Embedded. Successful                 attacks of this vulnerability can result in unauthorized ability to cause a partial denial of service (partial DOS) of                 Java SE, Java SE Embedded. Note: Applies to client and server deployment of Java. This vulnerability can be exploited                 through sandboxed Java Web Start applications and sandboxed Java applets. It can also be exploited by supplying data to                 APIs in the specified Component without using sandboxed Java Web Start applications or sandboxed Java applets, such as                 through a web service.
Java CVE-2020-14581Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE (component: 2D). Supported versions that are                 affected are Java SE: 8u251, 11.0.7 and 14.0.1; Java SE Embedded: 8u251. Difficult to exploit vulnerability allows                 unauthenticated attacker with network access via multiple protocols to compromise Java SE, Java SE Embedded. Successful                 attacks of this vulnerability can result in unauthorized read access to a subset of Java SE, Java SE Embedded accessible                 data. Note: Applies to client and server deployment of Java. This vulnerability can be exploited through sandboxed Java                 Web Start applications and sandboxed Java applets. It can also be exploited by supplying data to APIs in the specified                 Component without using sandboxed Java Web Start applications or sandboxed Java applets, such as through a web service.
Java CVE-2020-14621Vulnerability in the Java SE,  Java SE Embedded product of Oracle Java SE (component: JAXP). Supported versions that                 are affected are Java SE: 7u261, 8u251, 11.0.7 and 14.0.1; Java SE Embedded: 8u251. Easily exploitable vulnerability                 allows unauthenticated attacker with network access via multiple protocols to compromise Java SE, Java SE Embedded.                 Successful attacks of this vulnerability can result in unauthorized update, insert or delete access to some of Java SE,                 Java SE Embedded accessible data. Note: This vulnerability can only be exploited by supplying data to APIs in the specified                 Component without using Untrusted Java Web Start applications or Untrusted Java applets, such as through a web service.
Java CVE-2020-18197In xsltCopyText in transform.c in libxslt 1.1.33, a pointer variable isn't reset under certain circumstances. If the                 relevant memory area happened to be freed and reused in a certain way, a bounds check could fail and memory outside a                 buffer could be written to, or uninitialized data could be disclosed.

   

  

Issues fixed in version 08.1.02

           

You can find the problems, workarounds and fixes related to this release in the issue list.