Passer au contenu principal

What's the MAC address of a certain port of a HiOS device? - Base de connaissances / Products / HiOS - Belden Support Center

What's the MAC address of a certain port of a HiOS device?

The agent of a HiOS device is reachable and transmits packets with the basic MAC address printed on a label on the chassis and displayed in GUI and CLI.
The numerically first port gets as port MAC address the basic MAC address + 5. The other ports get the respective addresses in consecutive order.

Example:
Basic MAC: 00:11:22:33:44:00
1st port:      00:11:22:33:44:08
3rd port:      00:11:22:33:44:0A